Edit a port

Devices have ports that are associated with IP addresses, ports, and protocols. Devices that have a specific catalog number have a predefined number of ports with assigned protocols.
TIP: If a device does not have a catalog number,
FactoryTalk Policy Manager
adds it as a
Generic Device
. When a security policy model includes generic devices, configure the number of ports on the device.
  1. From the navigation bar, either:
    • Select
      Canvas
      and then select a device.
    • Select
      Zones
      and then select a zone and a device.
    • Select
      Devices
      and then select a device.
  2. In
    PROPERTIES
    , select the tab associated with the port to configure and edit the port properties.
    For more information, see Port properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal