Add a port

Add ports to generic devices to match the device configuration.
TIP: By default, each new generic device has a single unconfigured port. Use this procedure to add more ports.
  1. From the navigation bar, either:
    • Select
      Canvas
      and then select a device.
    • Select
      Zones
      and then select a zone and a device.
    • Select
      Devices
      and then select a device.
  2. In
    PROPERTIES
    , next to
    Ports
    , select
    +
    .
  3. In
    PROPERTIES
    , select the tab associated with the port to configure and edit the port properties.
    For more information, see Port properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal