Edit a conduit

Conduits allow trusted communication outside of zones. Conduits require two endpoints.
  1. From the navigation bar, select either
    Canvas
    or
    Conduits
    .
  2. Select the conduit to edit.
  3. Make changes in
    CONDUIT PROPERTIES
    .
    For more information, see Conduit properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal