Back up a policy model

Back up
FactoryTalk System Services
to save a copy of the policy model and its associated certificates.
  1. Open the command prompt as an Administrator.
  2. In the command prompt, enter
    cd "C:\Program Files (x86)\Rockwell Software\FactoryTalk System Services"
  3. Run the backup utility by entering one of these commands:
    • To create a plaintext backup of the data, enter
      FtssBackupRestore -B
    • To create an encrypted backup of the data, enter
      FtssBackupRestore -B -P
      password
      or
      FtssBackupRestore -B -P "
      password
      "
      This creates an encrypted backup of the data using the password supplied after the
      -P
      parameter. Quotation marks are optional. This password must be supplied to restore the data.
    The
    backup.zip
    file is created. Once performed, the
    FactoryTalk Services Platform
    Backup includes this file.
  4. Verify that the backup file is present in this location
    C:\ProgramData\Rockwell\RNAServer\Global\RnaStore\FTSS_Backup
    TIP: The
    ProgramData
    folder is hidden by default in
    Windows
    File Explorer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal