Secured device replacement
The secured device replacement process identifies onboarded devices against existing entries in the policy model based on the specific criteria and deploys the policies automatically.
The onboarding device matches the device in the policy model if the following properties are the same:
- IP address
- Vendor
- Product type
- Product code
- Major firmware revision (the same or higher)IMPORTANT: The vendor certificate of a device determines the vendor property. Currently,FactoryTalk Policy Managersupports onlyRockwell Automationvendor certificates.
Provide Feedback