Disable Automatic Policy Deployment
Disable Automatic Policy Deployment by editing global settings and manually closing ports on the machine.
TIP:
The
FactoryTalk Policy Manager
installation agent opens these Windows Firewall ports: UDP 5353
and TCP 40014
. To operate correctly, the Automatic Policy Deployment functionality requires these ports to be open.- OpenFactoryTalk Policy Manager, selectGlobal Settingsand clear theEnable automatic device discovery and onboardingcheckbox.
- Manually close theUDP 5353andTCP 40014ports on the machine.
Provide Feedback