Recipes editor

The recipes editor widget contains the graphical objects and NetLogics required to display and manage the recipes at runtime. The widget is available from the
Template Libraries
.
The recipes editor widget displays a Navigation Panel with the following tabs:
Recipes list
Displays a list of the available recipe schemas in a DataGrid. In this tab, you can use dedicated buttons to:
  • Refresh the list of recipes.
  • Open a side menu to activate, rename, duplicate or delete a recipe.
  • Create a new recipe or create a new recipe from target, such as a controller.
  • Go to the parameters for a specific recipe to edit its parameters.
Parameters list
You can modify the recipe parameter values of the recipe selected in the first tab. In this tab, you can also use dedicated buttons to:
  • Return to the recipes list panel.
  • Revert or save your current edits.
  • Apply your edits to the controller.
  • Read recipe values from the controller and load them as recipe parameters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal