OMRON Fins Driver
Observe these guidelines when working with the OMRON Fins Driver.
Supported controllers
The driver supports OMRON® CJ and CP controller families.
IMPORTANT:
The driver has been tested with CJ2 controllers family.
Controller tags import
You can only import tags from TXT files in the offline mode.
IMPORTANT:
Before you import tags into
FactoryTalk Optix Studio
, from CX-Programmer, copy the symbol table into a TXT file.For more information, refer to the product documentation.
Data types
Controller data type | FactoryTalk Optix data type | Length |
|---|---|---|
BOOL | BOOL | 1 BIT |
CHANNEL | INT16 | 2 BYTES |
COUNTER | INT16 | 2 BYTES |
WORD | UINT16 | 2 BYTES |
DWORD | UINT32 | 4 BYTES |
LWORD | UINT64 | 8 BYTES |
INT | INT16 | 2 BYTES |
DINT | INT32 | 2 BYTES |
UINT | UINT16 | 2 BYTES |
UINT_BCD | UINT16 | 2 BYTES |
UDINT | UINT32 | 4 BYTES |
UDINT_BCD | UINT32 | 4 BYTES |
LINT | INT64 | 4 BYTES |
ULINT | UINT64 | 8 BYTES |
ULINT_BCD | UINT64 | 8 BYTES |
REAL | FLOAT | 4 BYTES |
LREAL | DOUBLE | 8 BYTES |
TIMER | INT16 | 2 BYTES |
STRING | STRING | LENGTH |
ARRAY | Type[Length] |
Controller memory area | FactoryTalk Optix memory area | Notes |
|---|---|---|
CIO | CIO area | |
A | Auxiliary area | |
T | Timer | |
C | Counter | |
D | Data Memory | |
H | Holding area | |
W | Work area | |
Ex | EM area CurrentBank | Addresses memory location x in the current bank. |
Ex_y | EM area | Addresses memory location y in bank x. |
IR | Not supported | |
DR | Not supported | |
TK | Not supported |
Provide Feedback