Resource Meter Dashboard
Provides real-time data on energy consumption and demand from individual resource meters. This level allows for precise monitoring and analysis of energy usage for specific resources, helping to identify areas for improvement and ensuring accurate reporting.
Click
Resource meter
from the hierarchy list.The following table provides the list of charts available by default in the dashboard:
S.No | Chart/Widget Type | Description |
---|---|---|
1 | Total Consumption (Harmonized) | This chart shows the current range and past range, along with the last value and last updated time. |
2 | Consumption | The user can view the selected time period with the respective granularity on the X-axis and consumption on the Y-axis. This chart shows the energy consumption summary. |
3 | Demand Summary (Harmonized) | This chart shows the peak, minimum, and average demand values along with the last value and last updated time. |
4 | Demand | The user can view the selected time period with the respective granularity on the X-axis and demand on the Y-axis. This chart shows the demand summary. |
Refer to Dashboard Features section to manage the Resource Meter dashboard.
Related Information
:Provide Feedback