Delete Chart/Widget

  1. To remove the chart/widget from the dashboard, click the [] icon from the respective chart/widget.
  2. In the
    Delete Chart
    dialog box, click
    Delete
    .
    Delete Chart
    The "
    <Chart Name> remove successfully
    " message is displayed.
    NOTE:
    This change in the dashboard is not permanent. After logging out and logging back in, the default view with all widgets and charts will be restored.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal