Baseline
The Baseline tab is designed to support energy conservation efforts through precise baseline calculations and detailed analysis. It contains two sub-tabs:
- Baseline Calculator: This tab facilitates accurate baseline calculation using regression analysis. It enables users to establish baselines, forecast energy consumption, and assess the effectiveness of energy conservation measures.
- Baseline Analyzer: This tab allows users to observe deviations over a specified time frame. It displays the Actual vs Calculated Baseline Consumption graph, Cumulated Deviation, Average Deviation, and the Baseline Formula, providing a comprehensive view of baseline performance and deviations.
Provide Feedback