Reset (RES)
The RES instruction resets a TIMER, COUNTER, or CONTROL structure.
When true, the RES instruction clears these elements:
When using a RES instruction for a: | The instruction clears: |
|---|---|
TIMER | .ACC value to 0 control status bits to false |
COUNTER | .ACC value to 0 control status bits to false |
CONTROL | .POS value to 0 control status bits to false |
Available Languages
Ladder Diagram

Operands
IMPORTANT:
Unexpected operation may occur if:
- Output tag operands are overwritten.
- Members of a structure operand are overwritten.
- Except when specified, structure operands are shared by multiple instructions.
Ladder Diagram
Operand | Data Type | Format | Description |
|---|---|---|---|
Structure | TIMER CONTROL COUNTER | Tag | Structure to reset |
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
|---|---|
Prescan | N/A |
Rung-condition-in is false | Set Rung-condition-out to Rung-condition-in. |
Rung-condition-in is true | Set Rung-condition-out to Rung-condition-in. Reset the specified structure. |
Postscan | N/A |
Example
Ladder Diagram

Reset Example
In the preceding example:
when limit_switch_8 is enabled, reset counter_4
when limit_switch_5 is enabled, reset Timer_1
when limit_switch_6 is enabled, reset control_1
Provide Feedback