Not Equal To (NE)
When enabled, the NE instruction and the operator
test whether Source A is not equal to Source B.
Available Languages
Ladder Diagram

Structured Text
This instruction is not available in structured text.
TIP:
Use the
< >
operator with an expression to achieve the same result.
Refer to Structured Text syntax for more information on the syntax
of expressions and assignments within structured text. Operands
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Ladder Diagram
Numeric Comparison
Operand | Data Type | Format | Description |
|---|---|---|---|
Source A | SINT INT DINT LINT USINT UINT UDINT ULINT REAL LREAL | immediate tag | Value to test against Source B |
Source B | SINT INT DINT LINT USINT UINT UDINT ULINT REAL LREAL | immediate tag | Value to test against Source A |
String Comparison
Operand | Data Type | Format | Description |
|---|---|---|---|
Source A | String type | immediate literal value tag | String to test against Source B |
Source B | String type | immediate literal value tag | String to test against Source A |
Affects Math Status Flags
No
Major/Minor Faults
See
NE String Compare Flow Chart
for faults.See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
|---|---|
Prescan | N/A |
Rung-condition-in is false | Set Rung-condition-out to Rung-condition-in |
Rung-condition-in is true | Numeric compare: If Source A or Source B is NAN or Source A is not equal to Source B. Set Rung-condition-out to true else Clear Rung-condition-out to false. |
String compare: See NE String Compare Flow Chart .If output is false Clear Rung-condition-out to false else Set Rung-condition-out to true | |
Postscan | N/A |
Examples
Ladder Diagram

Structured Text
if value_1 <> value_2 then light_4 := 1; else light_4 := 0; end_if; if value_3 <> ’I am EQUAL’ then light_5 := 1; else light_5 := 0; end_if;
Provide Feedback