View parameters
The
Parameter
tab contains a list of all of the parameters associated with the selected step or procedure. If the selected recipe step is a phase, the phase parameters are displayed. If the selected step is an operation or unit procedure, the procedure’s parameters are displayed. If no recipe step is selected, the current procedures parameters are displayed.
Provide Feedback