View expression values
In the
Binding Requirement Expression Values
dialog box, a list of units is displayed that shows the potential legal binding candidates for a unit requirement. Each unit requirement displays: - The unit name
- The current value (TrueorFalse), which shows whether unit binding candidates meet the selected binding requirement
- The order of the units, based on the evaluation of the binding preference expressionsTIP:If all preferences evaluate equally, the unit list is displayed with the lowest to highest equipment IDs, which are defined in the Area Model.
- The current value, which dynamically updates as the inputs to the expression change, and which may reorder the units when the dialog box is closed and reopened
- An expression value indicating whether the binding candidates meet the selected binding requirementTIP:If{???}is displayed in the dialog box, an expression cannot be evaluated by theFactoryTalk BatchServer.
View expression values for unit binding requirements and preferences during batch execution.
To view expression values for unit binding requirements and preferences
- SelectBatches.
- Select the batch that has the unit requirement expression data you want to view.
- In theBatch Detaildisplay, do either of the following:
- For a unit procedure or an operation batch, select the procedure.
- For a batch procedure, select a step to see that step’s unit requirement, or select the procedure to see all unit requirements associated with the batch procedure.
- Select theBindingtab. Summary information for the unit requirements is displayed.TIP:To find a unit requirement in a list, select theFilterfield and enter information about the unit. You can filter unit requirements by name, type, and class/instance.
- Select the unit requirement.
- In theUnit Requirementdetails, underBinding Requirements, select either a binding requirement or a binding preference to display the real-time values of the expressions.
- For binding requirements, theBinding Requirement Expression Valuesdialog box is displayed.
- For binding preferences, theBinding Preference Expression Valuesdialog box is displayed.
- View the expression data.TIP:The current value updates in real-time.
- When finished, selectClose.
- In theUnit Requirementsdialog box, selectClose.
Provide Feedback