Information in the Equipment view

The Equipment view presents a set of data based on the selected level. Additional Phase Logic Interface (PLI) information is displayed as a tool tip when your cursor passes over an equipment module. The following is an overview of the data displayed within each level:
Information
Description
Area
Process
Cell
Unit
Phase
Batch ID
The Batch ID of the selected batch. In the Area display mode, there is a drop-down list containing the Batch IDs of all the batches on the Batch List in order by Create ID.
X
X
X
X
State-SI
The state of the phase along with the step index; only included in the Unit display mode.
X
State
The state of the selected batch. For example, RUNNING, HELD, etc.
X
X
X
X
Mode
For the Area and Process Cell displays, this is the mode of the selected batch. For example, O_AUTO, MANUAL, or S_AUTO. In the Unit display mode, this indicates ownership of the phase. For example, PROGRAM if the phase is under a batch's control, OPERATOR if the phase has been acquired by the operator and EXTERNAL if the external bit has been set.
X
X
X
X
Instructions
A link to the Instructions view. The instructions for the current batches within the area or process cell are included in the Instructions view.
X
X
Link1 - Link5
These customizable hyperlinks can be defined for each equipment resource in the equipment database. The labels (Link 1, Link 2, etc.) are also customizable for each
specific equipment resource type.
X
X
X
Request
A description of the unresolved request on the phase, if any.
X
X
Phase
The name of the phase.
X
Step Index
The step index of the phase.
X
Failure
Failure message, when appropriate.
X
Unit
Name of the unit in which the phase resides.
X
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal