Start a phase

Start a phase in the
Phase Control
window.
To start a phase:
  1. Open the
    Phase Control
    window.
  2. In the
    Phases
    area, select the appropriate phase and acquire FTB_VW_Phase Control Acquire_b the phase.
  3. Click
    Start
    ftb_vw_start_batch_bB12 to initiate the phase and then confirm the command.
  4. Type a unique batch ID for the manual phase control batch.
  5. (optional) If control strategies are enabled for the phase, select the appropriate control strategy from the
    Control Strategy
    list.
  6. Click
    OK
    .
    IMPORTANT:
    Batch IDs must be unique or the
    Arbitration
    window will not update correctly.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal