Perform semi-auto phase processing
You can manually step through a phase using SEMI-AUTO mode in the Equipment view, as long as the phase logic was programmed with break points. Semi-Auto processing allows you to test the functionality of the phase logic prior to releasing the phase for general use. When a phase is in SEMI-AUTO mode,
S
displays next to the step index on the phase button. PAUSED is displayed on the phase button in dark blue text, on the line between the phase’s name and its current state.
TIP:
The phase logic must set the Paused bit where
appropriate. These programmed break points are where the phase pauses while in Semi-Auto
processing.
- Open the Equipment view.
- Navigate to the unit in which the desired phase resides. Phases that are not running are in the IDLE state.
- Select the desired phase icon, and then click theAcquirebutton.
- Click outside of the phase icon. This enables theSemi-AutoandAutooptions in the Mode area.
- Select theSemi-Autooption to initiate semi-auto processing. The phase is automatically put into the PAUSED state, allowing the operator to manually process the phase using theResumecommand button.
- Click theStartbutton to initiate the phase. TheBatch IDdialog box opens.
- Type a uniqueBatch IDand then clickOKto continue. Respond to any prompts on the Instructions view.
- The phase pauses at each pre-programmed break point. Click theResumecommand button to restart execution of the phase. The phase transitions to the RUNNING state and then returns to the PAUSED state when it reaches the next pre-programmed break point. The phase transitions to the COMPLETE state after all steps have been executed.
- With the acquired phase icon selected, click theResetcommand button. The phase transitions to the IDLE state.
- Click theReleasecommand button. The Owner box is set back to blank, indicating that there is no current owner of the phase.
Provide Feedback