Restart a batch
Restarting a batch begins the execution of the batch that is in the HELD state. Unless there is an active step change, the batch restarts with the step that was the active step at the time the batch was HELD.
To restart a batch:
- In theBatch Listview, select the batch.
- (optional) Choose theSFC VieworTable View.
- Select the step you want to restart.
- The mode must be O-AUTO.
- ClickRestart BatchorRestart Step.
Provide Feedback