Place a batch in automatic mode

A batch or step that is in MANUAL mode must be placed in AUTOMATIC mode to continue normal execution. A batch or step may be placed in AUTOMATIC mode from the following
eProcedure
Client views: Batch List, Equipment and Procedure.
  1. Open the appropriate
    eProcedure
    Client view.
  2. Use the Filter view to select the batch that is to be placed in AUTOMATIC mode. To place the entire batch in AUTO mode, you should select the highest recipe level and place it in AUTOMATIC mode (i.e., unit procedure or procedure).
  3. Click the
    Auto
    command button. The batch will continue to sequence automatically.
  4. All higher level steps are left in MANUAL mode and all lower level steps are placed in AUTO mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal