Hold a batch
This command temporarily stops execution of the batch at a step. A HELD batch can be RESTARTED, STOPPED, or ABORTED. A batch can be held from the following
FactoryTalk Batch View
windows:- Batch List view
- Procedure as SFC view
- Procedure as Table view
To hold a batch:
- In theBatch Listview, select the batch.
- (optional) ClickProcedure as SFCorProcedure as Tableto select the view you want.
- Select the step you want to hold.
- The mode must be O-AUTO.
- ClickHold BatchorHold Step.
Provide Feedback