Command a batch in the Batch List view

You can issue Batch commands by using the command buttons in the Batch List view, Equipment view and the Procedure view. Only buttons representing valid commands are enabled. Some of the command buttons are toggles, meaning that the button label will change, depending on the state of the batch. For example, if a batch’s state is READY, the label on the
Start/Restart
button is
Start
. However, if the batch’s state is HELD, the button’s label is
Restart
.
Possible Batch States and Color Indicators
READY
Black
COMPLETE
Dark Gray
IDLE
Black
RUNNING
Dark Green
RESTARTING
Green
STARTING
Green
CONNECTING
Green
DOWNLOADING
Green
UPLOADING
Dark Green
UPLOAD_HELD
Dark Yellow
HOLDING
Yellow
HELD
Dark Yellow
STOPPING
Blue
STOPPED
Dark Blue
ABORTING
Magenta
ABORTED
Dark Magenta
Possible Modes in the Mode Column
O_AUTO
The batch is running normally and is under
FactoryTalk Batch
Server control. Operator intervention is not required to complete the batch.
MANUAL
The batch is running manually and is under operator control. When a batch is placed in Manual, the current step is completed and the batch waits for the operator to perform an active step change and/or return the batch to the Auto mode to continue.
S_AUTO
The batch is running normally and is under operator control. When a recipe level is placed in Semi-Auto, the current step is completed and pauses at the next transition as it becomes TRUE. The operator is required to issue the Resume command or return the batch to the Auto mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal