Batch List view command buttons

You can use the Batch List view to add a batch to and command batches on the Batch List. The Command area includes the command buttons that pertain to each Batch List view. If you wish to command a batch, you must first select the batch. The appropriate command buttons are then enabled, based on the state and mode of the selected batch. (See
Command area
for more information.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal