Information in the Batch List view

The Batch List view includes information regarding each batch that is on the Batch List. You can use the horizontal scroll bar to scroll right and left to view all of the columns of data. A vertical scroll bar is included if there are more batches on the Batch List than can display in the allotted area.
The following data is included in the Batch List view:
Item
Description
Batch ID
User-entered or automatically generated identification of the batch. Each Batch ID must be unique.
Recipe
Name of the recipe from which the batch was created.
Description
Description of the recipe.
Start Time
Time the batch was started.
Elapsed Time
Elapsed time measured from the start time, updated after completion
of a phase.
State
Current state of the batch.
Mode
Current mode of the batch.
Failure
Failure information for the batch.
Process Cell
Name of the process cell in which the batch is running.
Units in Use
Units currently in use by the batch.
Phases In Use
Phases the batch is currently running.
CreateID
Unique ID assigned by the
FactoryTalk Batch
Server to the batch when it is created.
Batches are listed in the Batch List view in alphanumeric order by Batch ID. You can toggle the order from ascending to descending by clicking on the Batch ID column heading. You also can sort batches on any other column heading by clicking on the desired column. When you exit
eProcedure
, the sort order reverts to the default alphanumeric order by Batch ID.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal