Use Open Platform Communications (OPC)

The
FactoryTalk Batch
Server supports the use of the Open Platform Communications (OPC) protocol. OPC provides a defined set of COM interfaces for data access functions.
The OPC communications protocol is used by the
FactoryTalk Batch
Server to communicate with process-connected devices via a data server and PC-Based phases. COM is used to communicate with other high-level applications such as
FactoryTalk Batch
Material Manager
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal