Create a shared directory
A shared directory allows computers on the network to read from and write to a common
recipe, area model, or data file. The
FactoryTalk Batch
installation creates a shared directory named BATCHCTL
where the FactoryTalk Batch
software is installed (the default is C:\Program Files (x86)\Rockwell
Software\Batch
). If you installed your project files in a different directory,
configure that directory as a shared directory. To configure a shared directory,
administrative privileges are required.To create a shared directory
:- Navigate to the project file directory, then right-click the folder, and select the sharing option.
- Use theFile Sharingdialog box to add each user or user group name that requires access to the project file directory.
- Repeat for each user or user group, including the user accounts used by theFactoryTalk BatchServer andFactoryTalk Event Archiver.
- SelectShare.
Provide Feedback