Determine abnormal termination

Upon startup, the
FactoryTalk Batch
Server reads the value of the AbnormalTermination field within the
Batchsvr.ini
file. If the field value is NO, or the field is not present, then no action is taken. If the field value is YES, then the current
Batchsvr.log
file is copied to the path specified by the ErrorLogDirectory entry in the
Batchsvr.ini
file. The name of the copied log file is determined based on the CopyFileID field.
After determining whether or not to make a copy of the current log file, the
FactoryTalk Batch
Server writes a value of YES into the field. At completion of a normal shutdown, the Server writes a value of NO into the field.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal