Control step reactivation error messages

These messages may appear when attempting to reactivate a control step:
Cannot reactivate step
Only past control steps that have not been reactivated, are in phases that are currently in the RUNNING state, and do not have any pending reactivated steps are eligible to be reactivated.
Cannot remove batch
If there are any incomplete Signature Requests pending for the batch, it cannot be removed from the batch list. Complete all Signature Requests and try again.
Permission Denied
If you do not have security permission to reactivate steps, you will see the "Permission denied to reactivate step" message. Another user with valid permission will have to reactivate the step.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal