Indicate a continuous phase

Simulate continuous phase logic by selecting
Continuous Phase
.
To indicate a continuous phase
:
  1. Start the
    FactoryTalk Batch
    Phase Simulator
    .
  2. Select
    Edit > Phase Configuration
    . The
    Phase Configuration
    dialog box opens.
  3. From the
    Select Phase
    list, select the appropriate phase.
  4. If this is a continuous phase, select
    Continuous Phase
    .
  5. Select
    Update Phase
    .
  6. Select
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal