Change the sequence of requests

Change the time, type, and parameters of the request in a phase.
To change the sequence of requests
:
  1. Start the
    FactoryTalk Batch
    Phase Simulator
    .
  2. Select
    Edit > Phase Configuration
    .
  3. In the
    Phase Configuration
    dialog box, from the
    Select Phase
    list, select the appropriate phase.
  4. Type an appropriate value in
    @Time
    (time is in seconds). This value determines when the request is processed. This value must not be greater than the
    Dwell Time
    .
    For example, if the
    Dwell Time
    is 30 seconds, and the
    @Time
    value is 20 seconds, then this request will be processed after the selected state has been active for 20 seconds.
  5. Type an appropriate request number in
    _RQ
    . (Refer to the
    FactoryTalk Batch
    PCD Programmer Technical Reference Guide
    for information on request numbers.)
  6. Type any required request parameter data in
    Q01
    ,
    Q02
    , and
    Q03
    . These parameters are used to further define the request.
  7. Select the
    Update Phase
    button.
  8. Select
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal