Work with manual instruction files

A manual instruction file is an HTML file that contains the control step(s) required to manually execute a phase within FactoryTalk Batch. The control step(s) display within FactoryTalk Batch View’s web-based client during recipe execution. Manual instruction files can include information such as operator instructions, batch-specific information, data entry fields for report values, and standard HTML components.
Create manual instruction files for each eProcedure or manual phase within the equipment database. Each time an instance of a phase is created, a manual instruction file must be associated with the new equipment module. Manual instruction files can be created using any text editor or HTML editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal