What is eProcedure?
e
Procedure?As one of the
FactoryTalk Batch
components, FactoryTalk
eProcedure
manages, sequences and documents the execution of manual operations. Automating batch
sheets and standard operating procedures (SOPs) through interactive web documents, eProcedure
provides the control needed to rapidly deploy new products into manufacturing and the
data collection necessary to achieve true plant floor to enterprise-wide integration. FactoryTalk
eProcedure
provides the benefits of procedure automation without the expense of equipment
automation. The FactoryTalk Batch
components incorporate the principles of batch and procedure automation, an approach
defined by ISA’s S88.01 standard.FactoryTalk
eProcedure
automation provides a means to automate the execution of procedural logic associated with
recipes, product grade changes, computer setup, and computer shutdown procedures. Operators
perform the actions on the equipment, but they are prompted and guided by eProcedure
. The procedure specifies the sequence and timing of actions that can be manually
performed or performed by automation equipment.Typical procedures that can be automated using
FactoryTalk
eProcedure
include:- Batch execution
- Equipment startup and shutdown
- Product changeover
- Abnormal condition handling
Provide Feedback