FactoryTalk Batch View
Use
FactoryTalk Batch View
to initiate and control the batch process. A batch is a running control recipe. The
material produced by a single execution of a recipe is also considered a batch. - UseBatchesto create, view, and command a control recipe, observe the execution of a single recipe, and bind units for class-based recipes. Once a control recipe is created, it remains in theBatcheslist until it is removed or until the FactoryTalk Batch Server is restarted with a cold boot. A graphical representation of a running batch and its associated data is displayed.
- UsePromptsto alert operators to value requests for parameters, unit binding, material binding, and signatures or manual instructions. A control recipe cannot complete execution until the operator provides the requested information. In most cases, pending requests for information (value prompts, signatures, or manual instructions) are not acknowledged until a user either provides the information or stops or aborts the control recipe.
- Value prompts alert operators to requests for parameter values, unit binding, and material phase/container binding.
- Signatures are requests for signoffs that require user permissions and optional comments. When a signature is generated against a control recipe, acknowledge the signature by completing the associated signoffs. The requested user information in a signature is determined by the signature template defined in the area model.
- Instructions are individual steps of a manually executed phase. As a batch executes, the instruction for each active step appears.Instructions execute in the order specified within the master recipe.
- UseEquipmentfor an equipment-centric view of the defined area model. There are three levels of equipment: process cell, unit, and phase.
- UseDiagnosticsto view server and service status, server performance, server statistics, arbitration, and journals.
- UseProfileto change the default language, view assigned groups,enable or disable the minimal view, and view authorization settings.
For more information on using these features, see
FactoryTalk Batch View
Help.Provide Feedback