FactoryTalk Batch Network Editor

The
FactoryTalk Batch
Network Editor is a utility that indicates where other
FactoryTalk Batch
and
FactoryTalk Batch
Material servers are located on the network. This network configuration allows for ease of integration with other
FactoryTalk Batch
components and simplifies the process of reconfiguring a multi-computer system. If
FactoryTalk Batch
Material Manager
is also installed the
FactoryTalk Batch
Network Editor is also used to indicate the location of the material database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal