Training the Component Baseline
To start training in FactoryTalk Analytics GuardianAI, the component should be running in normal operation. The FactoryTalk Analytics GuardianAI is designed to observe the component under normal usage and will train models across the various speeds of the operation.
Start Training and Monitoring
Click
Start Training and Monitoring
on the Training Page. The user
will see the progress bar begin to populate as data is acquired from the variable frequency
drive.The application will create a new model at each half-hertz increment of the operation speed
of the component. The model is automatically switched by reading the command frequency of
the drive. Once the number of training iterations is acquired, the given frequency bucket
will automatically switch from training to monitoring. Multiple frequencies can be trained
in parallel depending on the variability in speed of the application. FactoryTalk Analytics
GuardianAI is designed to switch automatically across frequencies between training and
monitoring.
While the component is training, the user cannot edit its configuration. To make any edits,
the user must click the
Stop Training and Monitoring
button.Training Baseline Component Behavior

Stop Training and Monitoring
Stop Training and Monitoring will stop training and monitoring the component. Once the user
stops training, any frequency bucket in progress will be reset back to 0%. Frequencies that
were already fully trained are preserved and will resume monitoring once the user starts
training again.
A dialogue box will prompt the user to accept the reset of the in-progress buckets and
confirm the action.
Stop Training Dialog Box

The user must stop training to make any edits to the component configuration.
Re-train Component
Re-training a component is essential if a major physical change is made to the system. An
example might be replacing the motor or full re-alignment of a coupling. FactoryTalk
Analytics GuardianAI starts the training process under normal conditions, but it is possible
there was already an existing degradation at the time when the baseline was acquired. In
this scenario, the application will monitor further degradation from baseline. If a user
makes a major physical change without re-training, there is a possibility that FactoryTalk
Analytics GuardianAI will view the normal operation as anomalous behavior. If too many false
positives are detected after a major maintenance event, then FactoryTalk Analytics
GuardianAI should be re-trained to acquire a new baseline of the component's behavior.
Provide Feedback