State Name
The tag value is shown as State name on the training page. If there is a change in the tag value coming from PLC, a separate tab is created for each state, using the tag value as the State name. For example, the tag selected during controller configuration is 'State A'. Hence, the state name is 'State A'.
State Name

Following is an example image where the component has multiple states.
Multiple States

In the above example, 'State C' is called the
Current State
. The name of the Current State is denoted with bold text and a blue border below it.If multiple state definition tags are selected on the
State Definition
page during controller configuration, the state name will be displayed as "<tag1-value><tag2-value>".Provide Feedback