Monitoring Status
On the Training page of a component, the user can view the following status in the Monitoring Status section:
- Controller Connection Status: When the Controller is configured, the status is displayed as green andController Connected. For the default state, it is displayed asController not configured.
- Controller path: The path of the controller is displayed. For the default state, it is displayed asN/A.
- Monitoring Tag status: When the monitoring tag is selected, the status is displayed as green andMonitoring tag on. For the default state, it is displayed as grey, andNo monitoring tag selected.
- Current Frequency: The current frequency at which the component operates is displayed.
- Current State: Name of the active state is displayed here. For the default state, it is displayed asN/A.
Monitoring Status

If only one tag is selected on the State Definition page, and if the tag is invalid, training and monitoring will be stopped. A message is displayed in red, as shown in the following image, and the current state will be shown as N/A.
If multiple tags are selected and all the tags are invalid, training and monitoring will be stopped.
Monitoring Status for Invalid Tags

Provide Feedback