Monitoring Workspace

The monitoring workspace, displayed in the following figure, provides quick access to the overall status of the components monitored by FactoryTalk Analytics GuardianAI.
  1. The left panel displays the different folders containing the component.
    • When a component in a folder encounters a deviation or failure risk, a tag on the folder illustrates the count of components encountering those events.
  2. The quick filters allow the user to gain additional insight into the components with a failure risk, deviation requiring labeling, or healthy components (no action required). Upon selecting a filter, only the components meeting the criteria are displayed.
  3. The detailed component page displays all information about the component, including a detailed view of deviations or failure risks requiring user action.
Component Monitoring Workspace
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal