Configuration Workspace

The configuration workspace, accessible from the monitoring workspace, is where users can create folders, add drives, define the component the drive is powering, and configure the training parameters. The workflow is designed with an easy-to-use stepper to guide the user in creating a new component for FactoryTalk Analytics GuardianAI to monitor.
Additionally, controller configuration is available for each folder to read the tags seamlessly and monitor multiple states of the component based on the state value coming from the PLC. The controller configuration is optional.
Configuration Workspace to Add a New Component
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal