Deviation to Failure Risk Workflow

This workflow is for new incoming deviations that have never been labeled within FactoryTalk Analytics GuardianAI. The FactoryTalk Analytics GuardianAI application is designed to learn new failure modes. Once a user has confirmed and labeled a deviation, each new occurrence of the same failure mode will surface as a failure risk.
Deviation to Failure Risk Workflow
As a new deviation is detected, FactoryTalk Analytics GuardianAI will have the following workflow:
  1. A deviation is detected with associated first principle recommendations.
  2. The user selects between the first principle, normal operation, or creates a new label.
  3. Once the detected deviation is labeled, the deviation will move to a failure risk.
  4. The user should select and resolve a failure risk once the issue is fixed on the physical system. If the issue is marked as resolved but it persists, FactoryTalk Analytics GuardianAI will re-surface the anomaly as a failure risk.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal