Notify Users and Recipients

FactoryTalk Analytics GuardianAI sends two types of notification emails.
Email Notification Frequency Configuration
  • Individual event notifications
    : These notifications are sent when a deviation or failure risk is detected on a component.
  • Summary notifications
    : These notifications are sent on a configured cadence regarding all active deviations and failure risks across all components monitored by FactoryTalk Analytics GuardianAI.
To enable individual event notifications, select the checkbox labeled
Send Immediately
. FactoryTalk Analytics GuardianAI sends email notifications for every deviation and failure risk event detected on all components under active monitoring.
To enable summary email notifications, select the dropdown under Notification Frequency to configure the cadence by which to send the summary emails, options include:
  • Disabled
    : Email summaries are disabled and will not be sent on any cadence.
  • Daily
    : Sent at 8 AM every day based on the time zone configured for the local installation of FactoryTalk Analytics GuardianAI.
  • Weekly
    : Sent at 8 AM every Monday based on the time zone configured for the local installation of FactoryTalk Analytics GuardianAI.
  • Monthly
    : Sent at 8 AM on the first Monday of every month based on the time zone configured for the local installation of FactoryTalk Analytics GuardianAI.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal