Notification Frequency
This topic provides information about the email notification frequency.
- Individual Notifications (if enabled)
- Deviations
- Each deviation will provide an email when generated.
- Subsequent grouped notifications will never generate an email.
- Failure Risks
- Moving a deviation to failure risk will not generate an immediate notification.
- Each failure risk will notify up to exactly 1 time per day if generated again.
- A failure risk will never notify on the same day it is converted to from a deviation.
- This means if the following occurs: Failure Risk Generated (email generated) -> Resolved -> Failure risk generates again (Same calendar day) the second generated risk would not trigger an email.
- Summary Notifications (all times local)
- Daily: 8 AM each day
- Weekly: 8 AM Monday
- Monthly: 8 AM first Monday
- If the application is restarted, the time to notify will always be the next notification point, starting from the next calendar day.
- Example: If the application is set to 'Daily', and the application restarts at 3 PM, it would generate at 8 AM the next day
- Example: If the application is set to 'Daily' and the application restarts at 7:55 AM, it would generate at 8 AM the next day (skipping the 8 AM 5 minutes from restart)
Provide Feedback