Summary Notification
The summary notification provides a high-level table regarding all unlabeled deviations and
unresolved failure risks for all components monitored by FactoryTalk Analytics GuardianAI. The
table rows will show the component names, with one row dedicated to each component. The table
columns include the count of unresolved Failure Risks ranked by severity, along with the count
of unlabeled existing deviations with the last column showing the time stamp of the last
detected event. Below the table is the enumeration of each component with additional details
regarding the detected failure risks and deviations.
Summary Notification

Provide Feedback