Single Event Notification

The single event notification is intended to send an immediate notification on any deviation or failure risk regarding a component monitored by FactoryTalk Analytics GuardianAI.
For a
deviation
, the notification contains the information shown in the following image.
Example of Deviation Notification Email
  • Component Name
    : Name of the component given during the first-time configuration.
  • Component Type
    : Pump, Fan, Blower, or Motor Analytics.
  • Folder Name
    : The folder name containing the drive and component combination.
  • Time Detected
    : The time at which the event was detected based on the local time zone of the FactoryTalk Analytics GuardianAI instance.
  • State
    : The state at which the component is operating.
  • Output Frequency
    : The output frequency of the drive.
  • Deviation
    : Name of the deviation
  • Percent above baseline
    : The percentage deviation from baseline.
  • Duration
    : Amount of time the deviation has persisted.
  • Probable Causes
    : First Principle Failure mode recommendations.
  • Number of recurrences
    : The amount of time the deviation has been detected.
For a
failure risk
, the notification contains the information shown in the following image.
Example of Failure Risk Notification Email
  • Component Name
    : Name of the component given during the first-time configuration.
  • Component Type
    : Pump, Fan, Blower, or Motor Analytics.
  • Folder Name
    : The folder name containing the drive and component combination.
  • Time Detected
    : The time at which the event was detected based on the local time zone of the FactoryTalk Analytics GuardianAI instance.
  • State
    : The state at which the component is operating.
  • Output Frequency
    : The output frequency of the drive.
  • Failure Risk Name
    : The name of the failure risk, this is given during the labeling process for a deviation.
  • Failure Risk Description
    : The description of the failure risk indicates additional details about the detected anomaly.
  • Failure Risk Prescription (if exists)
    : Recommendation regarding the action to take to resolve the failure risk.
  • Severity
    : A ranking of the severity (low, medium, high).
  • Time to Resolve
    : Time expected to resolve the failure risk.
  • Recurrence
    : The number of times the failure risk has been detected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal