Configuring SSL Certificate
By default, FactoryTalk Analytics GuardianAI is configured with a self-signed certificate. A secure sockets layer (SSL) certificate refers to a file hosted within the webpage's origin server, which holds the data that browsers access when you are viewing and interacting with the page. The certificate may be self-signed or signed (issued) by a third party. Customers can import an issued certification and import it by utilizing the Import SSL Certificate section.
General Settings - Import SSL Certificate

Provide Feedback