Configure Component

Perform the following steps to configure a new component:
  1. Provide the following details in
    Component
    section of
    Configuration
    :
    • Name of component
      : Provide a unique name for a component.
    • Select type of component
      : Select the type of component. One of Pump, Fan, Blower, Motor (used for other component types).
    • Manufacturer
      : Provide the name of the manufacturer. This is optional.
    • Serial number
      : Provide the serial number of the component. This is optional.
    • Model number
      : Provide the model number of the component. This is optional.
    • Part number
      : Provide the part number of the component. This is optional.
  2. Provide the following details in
    Bearing Monitoring
    section:
    • Inner race multiplier
    • Rolling element multiplier
    • Outer race multiplier
    • Cage multiplier
    For more details on these parameters, refer to Bearing Monitoring.
  3. Provide the following details in the
    Pump
    /
    Fan
    /
    Blower Specifications
    :
    NOTE: This option is visible only when you select the Pump, Fan, or Blower as the component type.
    • Number of blades
      : Provide the number of blades. The number of blades should be greater than or equal to 2 and less than or equal to 40.
Configure Component Parameters
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal