configwsmTLS
Use the
configwsmTLS
command on the FactoryTalk Activation Manager
server to
configure the certificate public key file (.cer), web socket port number, authentication
endpoint, and port that will be used to secure the connectino between clients and the
FactoryTalk Activation Manager
Websocket Service.These options are required:
- -w, --websocket
- -c, --certfile
- -p, --wssport
- -ap, --authendpoint
- -ae, --authport
Usage: configwsmTLS -w enable -c "C:\Certificates\certfile.cer" -p 5555 -ae
"https://example.com" -ap 443
This table describes the command options.
Option | Description |
|---|---|
-v|--verbose | Use this option to turn on trace messaging. Example: "-v" |
-w|--websocket | Enable or disable the Websocket Service. Allowed values: "enable" or "disable". Example: "-w enable" |
-c|--certfile | Configure the Websocket Service to use the specified certificate
exported public key file. Expected value: String, full path and file name. Example: "-c C:\Certificates\certfile.cer" |
-p|--wssport | Configure the Websocket Service to listen on the given port
number. Allowed values: Number between 1 and 65535. Example: "-p 5555" |
-ae|--authendpoint | Configure the Websocket Service to fetch an authentication token from
a FactoryTalk Web Service. Expected value: String, fully qualified domain name and URL. Example: "-ae https://example.com/endpoint" |
-ap|--authport | Configure the port number of the FactoryTalk Web Service
endpoint. Expected value: Number between 1 and 65535. Example: "-ap 443" |
-s|--status | Output the status of the Websocket Service. Example: "-s" |
-r|--restart | Enable and start, or restart the Websocket Service if currently
running. This also applies any recent configuration changes. Example: "-r" |
-?|-h|--help | Show help information. Example: "-h" |
Provide Feedback