A - B

activate
To make a Rockwell Software product active so that it can run without the limitations imposed by demonstration mode. Without activation, some Rockwell Software products will not run, some will run with diminished functionality, and others will run for a limited period of time and then shut down with or without warning.
activation host
The device associated with an activation by a unique ID.
activation server
An activation server is any computer that hosts concurrent activations. The activation server manages the activations and shares them with other configured computers on the network.
allocated
In the context of a borrow, a floating license has been loaned or checked out from the
FactoryTalk Activation
server to a specific machine. This reduces the Available Activations by 1.
binding
A virtual connection of two or more components in a system.
bound
A license has been linked to a computer, virtual machine, or dongle host ID. This reduces the activations available from
Rockwell Automation
products by 1.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal