Overview view parameters
The
Overview
view includes these parameters.Parameter | Description |
|---|---|
Device type | Displays the device catalog number and type. |
Vendor | Displays the device manufacturer information. |
Series | Displays the device series. |
Revision | Displays the device major and minor revisions. |
Electronic keying | Displays the electronic keying used for the device. |
Connection | Displays the connection to communicate with the device. |
Safety Relays | Displays the safety relays. |
Device definition | Opens Device definition to change the device values. |
Provide Feedback