Device Definition - New Relay dialog box parameters

The
Device Definition - New Relay dialog box
includes these parameters.
Parameters
Parameter
Description
Relay list
Select the model of Guardmaster Safety Relay (GSR) monitored by the communication interface device.
Slot
Assign a slot number to the GSR.
Slots are numbered left to right, where slot 1 should correspond to the relay to the immediate right of the communication interface device. The selections will generate the appropriate device-defined tag to match theĀ GSRĀ monitored by the GSR EtherNet/IP communication auxiliary device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal